You are here: Tools > Input Output Editor

Custom Input/Output Editor

The Input/Output Editor (hereafter I/O Editor) is a tool used to declare and set up I/O devices, and establish the link between the application variables and physical equipment. It shows a list of the currently defined I/Os.

To open the I/O Editor select Tools>Custom IO Editor from the menubar.

Input/Output Editor

Figure 10-39: Input/Output Editor

For the Description field, see format explanations.

Concept Link IconSee Also

 

Add Input Output

Modify Input Output

Delete Input Output


Stay Connected with Kollmorgen

Copyright © 2015 Kollmorgen™